==============================================================
2v0p1
==============================================================

Added Features:
 * Added board support: BRD4002B
 * General improvements for CLI commands.

Addressed issues:
 * Stored PTI configuration would not be applied on boot.

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
2v0p0
==============================================================

Added Features:
 * Added WinUSB support
     The driver mode will change to WinUSB automatically after the update.
     This will cause the USB PID to change, which may cause issues in special setups relying on the PID.
     For Windows 7 and earlier: Please install the latest SEGGER J-Link software pack
     with the "Legacy drivers" option enabled before installing this update.
     If needed, the mode can be changed back to SEGGER using either one of:
     - Simplicity Commander: "commander adapter drivermode" or GUI
     - Admin console: The "sys drivermode" command.
     - SEGGER J-Link Configurator
 * Enabled PCODE and HSS support
 * Updated bootloader to 0.13.0

Addressed issues:
 * Reading CTUNE value could return garbage if no value was set in the radio board

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v6p1
==============================================================

Added Features:
 * None

Addressed issues:
 * VCOM did not work in debug mode OUT or MINI. Introduced in 1.6.0.

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v6p0
==============================================================

Added Features:
 * Disable VCOM buffers when in debug mode "IN" to allow an external adapter to use the VCOM port
 * Added command to restore default configuration - "sys restore"
 * Added command to manually disable/enable VCOM - "serial vcom enable/disable"
 * Support controlling power on/off and voltage from PC tools

Addressed issues:
 * Fixed potential for corrupting configuration, including IP config
   * This release will automatically re-enable DHCP if both IP and netmask are configured to 0.0.0.0
 * Identification of radio boards could fail intermittently
 * Fix USB configuration during boot which could trigger an error on Windows
 * Improved PTI baud rate matching at 3.2 MBaud
 * Improved resistance against "garbage" UART bytes when VCOM is disabled
 * Concurrent use of RTT and VCOM could cause data loss on the VCOM channel.
 * Rapid duty cycling around 21 mA could cause NaN samples from AEM.
 * Connecting to port 4901 would fail in certain scenarios. Introduced in 1.5.1.
 * Series 1 device recovery was unreliable. Introduced in 1.5.1.

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v5p1
==============================================================

Added Features:
 * Support for reading and writing scratchpad from PC tools
 * Support reading MAC address from PC tools
 * By default, AEM is recalibrated when changing target voltage by more than 0.1 V
   * This can be disabled by passing "--nocalibrate" to the "target voltage" command
 * Support clearing the nickname by using syntax 'sys nickname ""'
 * Updated the base J-Link debugger application sources

Addressed issues:
 * None

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v5p0
==============================================================

Added Features:
 * Support for "auxillary UART" for SiWx917 devices, re-purposing flow control pins
 * Support for VCOM config from PC tools
 * Support starting AEM calibration from PC tools

Addressed issues:
 * None

Known Issues/Limitations:
 * VUART on series 2 devices may stop working after a reset of the the target device.


==============================================================
1v4p12
==============================================================

Added Features:
 * Force VCOM enable on for certain Si91x boards lacking HW support

Addressed issues:
 * VUART didn't work on certain xG24 projects
 * For a small set of radio boards, the stored CTUNE values were not exposed to external applications (e.g. Commander/Studio)

Known Issues/Limitations:
 * VUART on EFR32xG22/EFR32xG21 may stop working after a reset of the target device.


==============================================================
1v4p10
==============================================================

Added Features:
 * Increased maximum PTI packet length from 1024 B to 1950 B
 * When the reset button is pressed, the board controller refreshes the display
 * Added "sys voltage" CLI command to check VMCU, 5V, Vtarget and 3V3
 * Added "target ledstatus" CLI command to check status of LEDs
 * VUART over PTI is selected automatically on boot for Si91x boards 
 * The reported maximum target interface speed is now dependent on the type of interface (SWD, JTAG, C2)

Addressed issues:
 * Improved PTI capture stability

Known Issues/Limitations:
 * VUART on EFR32xG22/EFR32xG21 may stop working after a reset of the target device.


==============================================================
0v8p7
==============================================================
  * Automatic configuration of VCOM/PTI over SWO (CoS)
  * Full implementation of Logic analyzer
  * Preview support for VUART over PTI

  Known issues/Limitations:
  * Potential performance issues with PTI


==============================================================
0v8p6
==============================================================
  * Added support for PTI
  * Mock implementation of Logic analyzer

  Known issues/Limitations:
  * Potential performance issues with PTI


==============================================================
0v8p5
==============================================================
  * Use DCH message version 3 by default


==============================================================
0v8p4
==============================================================
  * Improved VCOM stability
  * Changed admin console prompt from WSTK to WPK
  * Added AEM calibration at boot
  * Fixed issues with timestamps leading to what appeared to be gaps in the AEM data
  * Fixed crash when running "pti config"

 Known issues/Limitations:
  * PTI is not supported yet
  * Logic analyzer is not supported yet


==============================================================
0v8p3
==============================================================
 * Improved VCOM stability
 * Fixed VCOM HW flow control
 * Fixed debug mode after boot - previously always booted in mode "MCU"
 * Fixed intermittent EEPROM write issue
 * Fixed initial IP config - now defaults to DHCP


==============================================================
0v8p2
==============================================================

 * Fixed SWO
 * AEM Gain values updated
 * Updated bootloader to 0.11.1


==============================================================
0v8p1
==============================================================

 * Support for nickname and IP configuration
 * AEM Gain values updated


==============================================================
0v8p0
==============================================================

Initial version